DriverOpenP (FUN)
FUNCTION DriverOpenP : CAA.HANDLE
See DriverOpenH for details. In contrast to DriverOpenH no dynamic memory will be allocated.
Memory specified by pMemory and szMemSize is used.
Use DriverGetSize to calculate the required memory size.
Please note that required memory size can change with new runtime version.
Note
pMemory should be aligned to a 4 byte address on 32 bit systems and an 8 byte address on 64 bit systems. To ensure this alignment, you can declare the memory with ARRAY [0..n] of __XWORD. Please keep in mind that the required memory size is different for 32 and 64-bit systems.
- InOut:
Scope
Name
Type
Comment
Return
DriverOpenPCAA.HANDLEhandle of CAN interface or
CAA.gc_hINVALIDif failed.Input
usiNetIdUSINTnumber of CAN interface [0..n]
uiBaudrateUINTBaudrate in kBit/s e.g. 1000 for 1 Mbit
xSupport29BitsBOOLFALSE: only 11-Bit IDs,TRUE: support also 29-BitszMemSizeCAA.SIZEsize of allocated memory
pMemoryCAA.PVOIDpointer to aligned memory
peErrorPOINTER TO ERROR
optional pointer to error enum