DriverGetSize (FUN)
FUNCTION DriverGetSize : CAA.SIZE
Calculates the needed memory size for DriverOpenP.
- InOut:
Scope
Name
Type
Comment
Return
DriverGetSizeCAA.SIZERequired memory size for DriverOpenP
Input
usiNetIdUSINTnumber of CAN interface [0..n]
xSupport29BitBOOLFALSE: only 11-Bit IDs,TRUE: support also 29-BitctMessagesCAA.COUNTnumber of transmit messages which should be allocated
peErrorPOINTER TO ERROR
optional pointer to error enum