TECT_RECIPE_STATUS (ENUM)

TYPE TECT_RECIPE_STATUS(

FB_NOT_RUNNING

TECT_RECIPE_STATUS shows the status of the recipe output function block

Attributes:
qualified_only
InOut:

Name

Initial

Comment

FB_NOT_RUNNING

0

1: Function block is disabled or no process running.

FB_BUSY

1

2: Function block is busy, either read or write process going on

PROCESS_COMPLETE

2

3: Recipe process is complete

OPERATION_WRONG_PARA

3

4: Wrong parameter at input Operation

NUM_OF_ZONE_WRONG_PARA

4

5: Wrong parameter at input NumberOfZone

TIMEOUT

5

6: Timeout of the recipe operation state

READ_DATA_FAILED

6

7: Read data failed: no correct format of data items.

ZONE_NO_MISMATCH

7

8: Mismatch in number of zones declared and zone data in recipe.

TIME_OUT

8

9: CAA file error: time limit exceeded

ABORT

9

10: CAA file error: Order has been aborted by activating input xAbort

HANDLE_INVALID

10

11: CAA file error: Invalid handle

NOT_EXIST

11

12: CAA file error: Directory or file does not exist

EXISTS

12

13: CAA file error: Directory or file already exists

NO_MORE_ENTRIES

13

14: CAA file error: No further entries are available

NOT_EMPTY

14

15: CAA file error: File or directory is not empty

READ_ONLY_CAA

15

16: CAA file error: Drive, file or directory is write protected

WRONG_PARAMETER

16

17: CAA file error: Wrong parameter

ERROR_UNKNOWN

17

18: CAA file error: Unknown Error

WRITE_INCOMPLETE

18

19: CAA file error: Not all data has been written

FILE_NOT_IMPLEMENTED

19

20: CAA file error: Function is not implemented

ASM_CREATEJOB_FAILED

20

21: CAA file error: Job creation of AsyncManager failed

FILE_OPERATION_DENIED

21

22: CAA file error: No access due to ForceFilePath/ForceIecFilePath

FIRST_MF

22

23: CAA file error: First manufacturer-specific error

LAST_ERROR

23

24: CAA file error: Insert manuf. specific errors here

ACTUAL_ZONES_LESS

24

25: Number of zones configured is more than the actual number of Zones