AUTOTUNE_ERROR_ID (ENUM)
- TYPE AUTOTUNE_ERROR_ID(
NO_ERROR
Enumeration of the Autotune Error ID, describes the details of each error generated by function block when auto tune fault occurs
- Attributes:
qualified_only- InOut:
Name
Initial
Comment
NO_ERROR
16#0
1: No Error
STEP_CHANGE_SMALL
16#72C0
2: The step change (Sp-Pv) was too small when adaption was started, a value of 120*Range/ Resolution is required as a minimum change.Resolution: 4096, Range: tsMachineSet.rTcMax * tsInternalStatus.iRawFactor.
INSUFFICIENT_MEASUREMENT_INTERVALS
16#72C1
3: Not enough measured points to calculate the tangent => increase the step change/decrease the scan time
DELAY_TIME_SMALL
16#72C2
4: Delay time could not be measured, probably too small
ADAPTION_LONG
16#72C3
5: Adaption needs too long (any time measured >32700 => increase the scan time/increase the value for CvAdapt .