DirRemove (FB; Prefix fildrm)
FUNCTION_BLOCK DirRemove EXTENDS CBM.ETrigToA
- InOut:
Scope
Name
Type
Comment
Inherited from
Input
xExecuteBOOLRising edge: Action startsFalling edge: Resets outputsIf a falling edge occurs before the function block has completed its action, the outputs operate in the usual manner and are only reset if either the action is completed or in the event of an error. In this case, the corresponding output values (xDone,xError) are present at the outputs for exactly one cycle.ETrigToA
xAbortBOOLTRUE: Action is stopped immediately and all outputs are reset to their initial values.ETrigToA
udiTimeOutUDINTDefines the time (µs) after which an FB (e.g. requiring an external acknowledgement) aborts operation due to a timeout with error message.
ETrigToA
Output
xDoneBOOLTRUE: Action successfully completedETrigToA
xBusyBOOLTRUE: Function block activeETrigToA
xErrorBOOLTRUE: Error occurred, function block aborts actionFALSE: No errorETrigToA
xAbortedBOOLTRUE: Action aborted by userETrigToA
Input
sDirNameCAA.FILENAMEDirectory name
xRecursiveBOOLTRUE: Remove all files and sub-directories, FALSE: Directory is only deleted, if empty, i.e. if no files and sub-directories are left; otherwise an error will be dumped
Output
eErrorLocal library error ID (5107 - FILE_NOT_EMPTY: Directory not empty; will be generated only if xRecursive = FALSE)