DirOpen (FB; Prefix fildop)
FUNCTION_BLOCK DirOpen EXTENDS CBM.ETrig
This function block opens a directory. The entries (files and sub-directories) of which should be read with the help of the function block ”FILE.DirList”. The return value is a handle. There may be restrictions concerning the specification of the directory name, e.g. only capital letters allowed, for different targets. The function ”FILE.GetProperty” shows these restrictions.
- InOut:
Scope
Name
Type
Comment
Inherited from
Input
xExecuteBOOLRising edge: Action startsFalling edge: Resets outputsIf a falling edge occurs before the function block has completed its action, the outputs operate in the usual manner and are only reset if either the action is completed or in the event of an error. In this case, the corresponding output values (xDone,xError) are present at the outputs for exactly one cycle.ETrig
Output
xDoneBOOLTRUE: Action successfully completedETrig
xBusyBOOLTRUE: Function block activeETrig
xErrorBOOLTRUE: Error occurred, function block aborts actionFALSE: No errorETrig
Input
sDirNameCAA.FILENAMEDirectory name, absolute or relative path specification
Output
eErrorLocal library error ID (0: no error; 5101: time out)
hDirCAA.HANDLEDirectory handle