DirCreate (FB; Prefix fildcr)
FUNCTION_BLOCK DirCreate EXTENDS CBM.ETrig
This function block creates a sub-directory in the standard directory. If the sub-directory already exists, an error message is generated. There may be restrictions concerning the specification of the directory name, e.g. only capital letters allowed, for different targets. The function ”FILE.GetProperty” shows these restrictions.
- InOut:
Scope
Name
Type
Comment
Inherited from
Input
xExecuteBOOLRising edge: Action startsFalling edge: Resets outputsIf a falling edge occurs before the function block has completed its action, the outputs operate in the usual manner and are only reset if either the action is completed or in the event of an error. In this case, the corresponding output values (xDone,xError) are present at the outputs for exactly one cycle.ETrig
Output
xDoneBOOLTRUE: Action successfully completedETrig
xBusyBOOLTRUE: Function block activeETrig
xErrorBOOLTRUE: Error occurred, function block aborts actionFALSE: No errorETrig
Input
sDirNameCAA.FILENAMEName of the new directory, absolute or relative path specification
xParentBOOLCreate missing subdirectories; TRUE: missing sub-directories will be created automatically, FALSE: missing sub- directories will cause an error message
Output
eErrorLocal library error ID (5104 - FILE_NOT_EXIST: Directory does not exist; 5105 - FILE_EXIST: Directory already exists )