DirCopy (FB; Prefix fildcp)
FUNCTION_BLOCK DirCopy EXTENDS CBM.ETrig
This function block copies the contents of the source directory to the destination directory Nonexisting destination path will be created. Depending of the parameters, all subdirectories and its content will be copied too, and existing files will be overwritten. NOTE: Empty direcories will be copied if xRecursive is TRUE.
- InOut:
Scope
Name
Type
Comment
Inherited from
Input
xExecuteBOOLRising edge: Action startsFalling edge: Resets outputsIf a falling edge occurs before the function block has completed its action, the outputs operate in the usual manner and are only reset if either the action is completed or in the event of an error. In this case, the corresponding output values (xDone,xError) are present at the outputs for exactly one cycle.ETrig
Output
xDoneBOOLTRUE: Action successfully completedETrig
xBusyBOOLTRUE: Function block activeETrig
xErrorBOOLTRUE: Error occurred, function block aborts actionFALSE: No errorETrig
Input
sDirNameDestCAA.FILENAMEdestination directory name
sDirNameSourceCAA.FILENAMEsource directory name
xRecursiveBOOLTRUE: all subdirectories and their contents are copied, FALSE: subdirectories are omitted
xOverWriteBOOLTRUE: existing files are overwritten, FALSE: existing files are left untouched
Output
eErrorLocal library error ID (0: no error; 5101: time out)