DirList (FB; Prefix fildls)
FUNCTION_BLOCK DirList EXTENDS CBM.ETrig
This function reads directory entries. The function block needs a valid handle which identifies the directory as a transfer parameter.
The information is written to structure ”deDirEntry” of type ”FILE_DIR_ENTRY”. If the function block cannot find any further entries
the error message ”ERROR.NO_MORE_ENTRIES” is generated and the entries in the structure ”deDirEntry” are deleted.
- InOut:
Scope
Name
Type
Comment
Inherited from
Input
xExecuteBOOLRising edge: Action startsFalling edge: Resets outputsIf a falling edge occurs before the function block has completed its action, the outputs operate in the usual manner and are only reset if either the action is completed or in the event of an error. In this case, the corresponding output values (xDone,xError) are present at the outputs for exactly one cycle.ETrig
Output
xDoneBOOLTRUE: Action successfully completedETrig
xBusyBOOLTRUE: Function block activeETrig
xErrorBOOLTRUE: Error occurred, function block aborts actionFALSE: No errorETrig
Input
hDirCAA.HANDLEDirectory handle
Output
eErrorLocal library error ID (5106 - FILE_NO_MORE_ENTRIES: no further entries available)
deDirEntryDirectory entry