CAA SerialCom (LIB)
- Version
3.5.17.0
- Namespace
COM
- Author
3S - Smart Software Solutions GmbH
- Placeholder
CAA SerialCom
Description 1
This library provides function blocks for using serial ports.
As the standardized in- and outputs of the function blocks are described in detail within the CAA Guidelines, this item will be omitted here.
Access to a COM device can be activated and configured with the help of COM.Open. The function blocks COM.Write and COM.Read allow writing and reading of data via the serial port. Having read out or written all data the serial port has to be released for other applications by use of COM.Close.
All input parameters of the function blocks are stored in local internal variables. This does not apply for the content of input data structures being referenced by a pointer, e.g. pBuffer of COM.Read or COM.Write.
Contents:
Indices and tables
- 1
- Based on CAA SerialCom.library, last modified 20.04.2021, 14:21:29. LibDoc 4.6.0.0-r.29The content file CAA SerialCom.library.json was generated with CODESYS V3.5 SP16 Patch 3 on 20.04.2021, 14:21:29.