DEVICE_STATE (ENUM)
TYPE DEVICE_STATE :
This enumeration lists all possible states of a device. The mapping to the according fieldbus specific states is defined by the associated fieldbus stack.
- Attributes:
qualified_only- InOut:
Name
Comment
UNKNOWN
The device state is unknown.Example: No supervision mechanism active.STOPPED
The device is stopped.
RUNNING
The device is running.
ERROR
The device is in error state.GetDeviceError may supply a specific error code.DISABLED
The device is disabled in device tree.
NOT_CONFIGURED
The device has not yet been configured by the stack.Example: Configuration phase not started yet.CONFIGURED
The device has been configured by the stack.Example: Configuration phase finished but device is not in running state.NOT_FOUND
The device was not found on bus.