GetDeviceError (FB)
FUNCTION_BLOCK GetDeviceError EXTENDS ETrigA
If IDevice.GetDeviceState returns DEVICE_STATE.ERROR this function block returns the associated device error code. The error codes are fieldbus specific and will be defined by the associated communication stack.
Note
This feature may not be supported by all fieldbus drivers.
eError will return ERROR.NOT_SUPPORTED if not supported.
- InOut:
Scope
Name
Type
Comment
Inherited from
Input
xExecuteBOOLRising edge: Action startsFalling edge: Resets outputsIf a falling edge occurs before the function block has completed its action, the outputs operate in the usual manner and are only reset if either the action is completed or in the event of an error. In this case, the corresponding output values (xDone,xError,iError) are present at the outputs for exactly one cycle.ETrigA
xAbortBOOLTRUE: Action is stopped immediately and all outputs are reset to their initial values.ETrigA
Output
xDoneBOOLTRUE: Action successfully completedETrigA
xBusyBOOLTRUE: Function block activeETrigA
xErrorBOOLTRUE: Error occurred, function block aborts actionFALSE: No errorETrigA
xAbortedBOOLTRUE: Action aborted by userETrigA
Input
itfNodedevice node
Output
eErroroperation error code
einDeviceErrordevice error code