PROC_CMD (ENUM)
TYPE PROC_CMD :
This enumeration is used when working with asynchronous methods. The current state is issued with the data structure PROC_STATE
- Attributes:
qualified_only- InOut:
Name
Initial
Comment
NONE
0
Operation is not started and stays in IDLE mode. The operation is returned to its initial state.
EXECUTE
Operation is started upon a rising edge and executed as long as the input remains on EXECUTE. The operation is done as soon as the output is assigned the value PROC_STATE.DONE.
ABORT
Operation is aborted. The abort is done if the state is assigned the value PROC_STATE.ABORTED.