BUS_STATE (ENUM)
TYPE BUS_STATE :
This enumeration lists all possible states of a fieldbus. The mapping to the according fieldbus specific states is defined by the associated fieldbus stack.
- Attributes:
qualified_only- InOut:
Name
Comment
UNKNOWN
The bus state is unknown.
STOPPED
The fieldbus is stopped. No I/O transfer can be processed.
RUNNING
The fieldbus is running.
ERROR
The fieldbus is in error state. GetBusError supplies the specific error code.
DISABLED
Bus is disabled in device tree.