Constants (GVL)

InOut:

Scope

Name

Type

Initial

Comment

Constant

gciMaxReadCamPoints

INT

256

the maximum number of cam points can be loaded by MCA_ReadCamFile.

gciMaxReadTappetPoints

INT

256

the maximum number of tappet actions can be loaded by MCA_ReadCamFile.

gciMaxWriteCamPoints

INT

256

The maximum number of cam points can be wroten into CamTable by MCA_WriteCamTablePoint.

gciMaxModifiedCamTable

INT

20

The maximum number of cam tables that can be modified by a instance of MCA_WriteCamTablePoint.

gciCamEditorDisplayPoints

INT

200

The number of points of curves that are shown in the visualization of MCA_VISU_FB_CamEditor_ABB_Horizontal/MCA_VISU_FB_CamEditor_ABB_Vertical.

gciCamEditorUndoSteps

INT

100

The number of steps that can be undone in the visualization of MCA_VISU_FB_CamEditor_ABB_Horizontal/MCA_VISU_FB_CamEditor_ABB_Vertical.