SntpSourceState (ENUM)
TYPE SntpSourceState
SntpSourceState is an enumeration type use to describe the several states of a time source
- Attributes:
qualified_only- InOut:
Name
Initial
Comment
SRC_STATE_UNKNOWN
0
state of source is unknown
SRC_STATE_CURRENT_SYNCED
1
indicates the source to which the sntp client is currently synchronized too
SRC_STATE_COMBINED
2
acceptable source which is combined with the selected source
SRC_STATE_NOT_COMBINED
3
acceptable source which is excluded by the combining algorithm
SRC_STATE_UNREACHABLE
4
the connection to the source is lost
SRC_STATE_ERROR
5
indicates an source which has an error
SRC_STATE_TOO_VARIABLE
6
the time of the source is too variable