NtpSourceState (ENUM)

TYPE NtpSourceState

NtpSourceState is an enumeration type use to describe the several states of a time source

Attributes:
qualified_only
InOut:

Name

Initial

Comment

SRC_STATE_UNKNOWN

0

state of source is unknown

SRC_STATE_CURRENT_SYNCED

1

indicates the source to which the sntp client is currently synchronized too

SRC_STATE_COMBINED

2

acceptable source which is combined with the selected source

SRC_STATE_NOT_COMBINED

3

acceptable source which is excluded by the combining algorithm

SRC_STATE_UNREACHABLE

4

the connection to the source is lost

SRC_STATE_ERROR

5

indicates an source which has an error

SRC_STATE_TOO_VARIABLE

6

the time of the source is too variable