ITrendStorageWriter.Initialize (METH)
METHOD Initialize
This method performs some initialization.
- InOut:
Scope
Name
Type
Comment
Input
udiRecordingTimespanUDINTThe configured timespan between two recordings
udiCountCyclesToStoreUDINTThe number of cycles, that have to stored in the temporary buffer before writing the data to the trend storage
udiMaxRecordCountUDINTIf this parameter has a value != 0 it indicates the maximum number of records, that will be stored in the trend storage. In case of 0 no limit exists
itfTrendRootPageManagerAn already initialized instance of ITrendRootPageManager, that is able to provide the root pages for tables and indexes