ETrendStorageReaderErrors (ENUM)
TYPE ETrendStorageReaderErrors :
This enumeration defines the errors, that can occur during accessing the trend storage using the public interface. Note: Error codes from 30400 to 30549 represent errors from the underlying
CAA Storage component. See STO.ERROR
- Attributes:
qualified_only- InOut:
Name
Initial
Comment
NoError
CmpErrors.Errors.ERR_OK
No error
NotInitialized
CmpErrors.Errors.ERR_NOTINITIALIZED
Required initialization was not done
WrongParameter
CmpErrors.Errors.ERR_PARAMETER
A required parameter is invalid, e.g. NULL is passed, where an instance is required
NoMemory
CmpErrors.Errors.ERR_NOMEMORY
Unable to allocate an internally used buffer resp. unable to store a value
NoObject
CmpErrors.Errors.ERR_NO_OBJECT
The specified object was not found
AdditionalReadCallRequired
CmpErrors.Errors.ERR_PENDING
This is not really an error, but the information, that all the data cannot be read by a single call and additional method calls are necessary
InvalidCall
20002
The call to a method is invalid, because this method cannot be called in this context.