VisuCommandInterface (LIB)

Version

4.5.0.0

Author

CODESYS Development GmbH

Placeholder

VisuCommandInterface

Description 1

This library provides a chance for other components (like the recipemanagement) to add the implementation of intern commands to the command manager of the visualization

Contents:

Indices and tables

1
Based on VisuCommandInterface.library, last modified 13.12.2023, 11:06:14. LibDoc 4.6.0.0-r.29
The content file VisuCommandInterface.library.json was generated with CODESYS V3.5 SP16 Patch 3 on 13.12.2023, 11:06:15.