TrendFbDatabaseAccessErrorHandler (FB)

FUNCTION_BLOCK TrendFbDatabaseAccessErrorHandler

This function block performs the error handling for all access to the underlying SQLite database

InOut:

Scope

Name

Type

Comment

Input

m_uiDiskFullDatabaseAccessSuspendTime

UINT

This member defines the behaviour of access to the underlying SQLite database in case of a ‘disk full’ event (normally indicated by an error code SQLITE_IOERR). 0: Starting from the first occurrence of an error code SQLITE_IOERR no more database access will be performed A positive value N: Starting from the first occurrence of an error code SQLITE_IOERR no more database access will be performed for N seconds

Methods:

ErrorHandling

IsDatabaseAccessEnabled

SQLiteErrorHandling

prvGetActionName

prvGetErrorDescription

prvGetFunctionName

Structure: