OBIO_PTOMotionKernel.ACTION_PTO (ACT)
the minimum possible frequency depends on the maximum required frequency. max possible frequency should have a 1% accuracy. divider is 16 bit. if the minimum frequency from parameter structure is higher, this value will be used. This will result in a better accuracy for max_frequency