OBIO_PTOMotionKernel (FB)
FUNCTION_BLOCK OBIO_PTOMotionKernel EXTENDS CMC_Basic_Kernel IMPLEMENTS iPTOKernel
This function block extends the basic motion kernel functionality, so that it can be used for the eco PTO outputs and connect a stepper drive.
2 axes are possible in total. For each axis one instance of this function block must be called.
Different parameters related to the PTO can be adjusted in OBIO_PTO_Motion_Parameter
It is possible to use either the stepper pulses as actual position, or connect a seperate value to Drive_ActualPosition
Note
Adjust PTO related parameter in OBIO_PTO_Motion_Parameter
The function block behaves as follows:
If the input Drive_InOperation is not connected, the required state is created internally.
If a drive delivers a corresponding signal, the Drive_Release/Drive_InOperation sequence can be used as with CMC_Basic_Kernel.
If the input Drive_ActualPosition is not connected, the stepper pulses can be used instead.
The input Drive_ActualPosition can be connected to an external encoder position value. (configure in OBIO_PTO_Motion_Parameter)
Note
The function block connects internally to the PTO outputs. The PTO configuration for the output is required, but no seperate function block to use PTO outputs.
Note
PTO parameters and input Enable_Virtual is not recommended to change on the fly or running system. This can lead to unexpected behavior of the system.
Note
This function block supports the visualization “CMC_VISU_FB_Basic_Kernel” from the ABB_MotionControl_AC500 library. User needs to manually map the instance of function block in Visualization reference.
- InOut:
Scope
Name
Type
Initial
Comment
Output
PTO_ErrorIDAC500_OnboardIO.Error_ID0
Error code. For error details refer to AC500_OnboardIO library Enum Error_ID
Inout
PTO_Motion_ParameterSpecific parameter set for PTO axis
Methods:
getBaseCounter
Structure: