LogGeneric_Output (FB)

FUNCTION_BLOCK LogGeneric_output EXTENDS AbbLConCA

This Function Block provides a decoded dataset of the corresponding data types from the SRAM-FIFOout of the Datalogger. The Function Block does not cover the transmission of the dataset. But it provides an interface for the user on which the data can be read and send according to application specific requirements and protocols.

The Function Block automatically reads the oldest dataset at a filling level of FIFOout > 0. Then the Function Block decodes the dataset from *.csv format and provides it to the outputs. The Function Block signals its availability through Done = TRUE and State = zLOG_OUTPUT_DATA_AVAILABLE. If this dataset is processed by the user, the user will have to signal this by Sent = TRUE to the Function Block. By the edge 0/1 the RAM-FIFOout is decremented by the value 1, Done changes to “FALSE” and on the output State the text “zLOG_OUTPUT_DATA_HAS_BEEN_SENT” appears. By a 1/0 edge on Sent the Function Block reads the next dataset (which is the same as the self triggered read without command, as long as Sent = false). This happens until FIFOOUT_LEVEL=0” and the Function Block signals “EMPTY”. At the same time at output State the message “zLOG_FIFOOUT_EMPTY” is given and all output values are deleted. While existing communication and exhausted FILE-FIFO the datasets, newly written by LogGeneric_Input to the FIFOin are continuously copied by the LogHandling directly to the FIFOout, as soon as there is space in the FIFOout for new datasets. For this the FIFOout should not be empty (EMPTY). It is different when FILE-FIFO is not empty. In this case at first FIFOout is fully decremented until FIFOOUT_LEVEL=0 and the Function Block signals “EMPTY”. After that a new dataset block is copied from FILE-FIFO into FIFOout.

../../../../../_images/LogGeneric_Output.jpg
InOut:

Scope

Name

Type

Initial

Comment

Input

PickedUp

BOOL

2: Feedback from Scada, that the data set has been received by the Scada station and that it is ready for the next data set

Done changes to “FALSE” and on the output State the text “zLOG_OUTPUT_DATA_HAS_BEEN_PICKED_UP” appears. By the 1/0 edge on PickedUp the Function Block reads the next dataset it is the same as the automatic reading without a command, as long as PickedUp = FALSE

Output

Done

BOOL

FALSE

2: Execution finished when output Done = TRUE

ErrorID

ERROR_ID

NO_ERROR

4: Shows error, Refer ERROR_ID enumeration for details of the error

State

zLOG_ENUM_STATE

zLOG_IDLE

5: Actual State of LogOutput, Enumeration of Type zLOG_ENUM_STATE

Empty

BOOL

FALSE

6: Output Buffer empty

FifoOutLevel

DINT

0

7: Level of FIFOout (maximum 161)

Id

STRING(8)

‘’

8: Output of the ID or name of the dataset as string chain (no special characters), maximum 8 characters

Timestamp

DT

9: Output of the time stamp of the dataset in the format year-month-day-hour-minute-second

Msec

UINT

0

10: Output of the milliseconds of the time stamp of the dataset

DataType

BYTE

0

11: Possible Data type’s: 1=BOOL, 2=BYTE, 3=INT, 4=UINT, 5=DINT, 6=UDINT, 7=REAL

BoolArray

ARRAY [0..iMaxARRAY_BOOL] OF BOOL

12: ARRAY[0..57], specified through input DATA_TYPE

ByteArray

ARRAY [0..iMaxARRAY_BYTE] OF BYTE

13: ARRAY[0..87] ,specified through input DATA_TYPE

IntArray

ARRAY [0..iMaxARRAY_INT] OF INT

14: ARRAY[0..49], specified through input DATA_TYPE

UintArray

ARRAY [0..iMaxARRAY_WORD] OF UINT

15: ARRAY[0..57], specified through input DATA_TYPE

DintArray

ARRAY [0..iMaxARRAY_DINT] OF DINT

16: ARRAY[0..28], specified through input DATA_TYPE

UdintArray

ARRAY [0..iMaxARRAY_DWORD] OF UDINT

17: ARRAY[0..30], specified through input DATA_TYPE

RealArray

ARRAY [0..iMaxARRAY_REAL] OF REAL

18: ARRAY[0..26], specified through input DATA_TYPE

Length

INT

0

19: Valid length of data in dataset

NumberItems

UDINT

0

20: Number of items since Enable=TRUE

Methods:

B_CyclicAction

D_AbortAction

E_ResetAction

Structure: