DataLogger (LIB)
- Version
1.0.0.17
- Namespace
AC500_DataLogger
- Author
None
- Placeholder
AC500_DataLogger
Description 1
The Datalogging function block library (PS5609-Log) contains five function blocks for the purpose of advanced time-stamped data logging for different use cases. In the most challenging use case it also can be called buffering: The AC500 application program generates data which are normally transmitted to a telecontrol system for storage and further processing or displaying to the end user. Typically, these may be remote applications like water- or oil-pumping or electrification stations or solar power plants. The connection between these remote stations with an AC500 and a central SCADA/telecontrol station is not always stable or only sporadically connected. Sporadically connected can be by intention, e.g. to save communication costs or open ports/connections to be used with a control station only in a limited way, then the Datalogging function blocks buffer or store data in case of a broken or intentionally interrupted connection between AC500 and the telecontrol system
Copyright: We reserve all rights in these programs and the information therein. Reproduction, use or disclosure to third parties without express authority is strictly forbidden. (c) 2006-2023 ABB, all rights reserved
Contents:
EnumsFunction BlocksInternal subroutinesLogGeneric_Input(FB)LogGeneric_Output(FB)LogHandling(FB)LogHandling.ActionBuildFilenames(ACT)LogHandling.ActionDirectCommunication(ACT)LogHandling.ActionFileDelete(ACT)LogHandling.ActionFileManager(ACT)LogHandling.ActionFileMove(ACT)LogHandling.ActionFormatDisk(ACT)LogHandling.ActionReadFromFile(ACT)LogHandling.ActionSecureRead(ACT)LogHandling.ActionWriteInFile(ACT)StateMachine
LogIec60870_Input(FB)LogIec60870_Output(FB)
GlobalConstantsGlobalTextList(Text List)GlobalVariablesImagesStructsVisualizationhistory(STRUCT)
Indices and tables
- 1
- Based on ABB_DataLogger_AC500.library, last modified 21.11.2023, 17:04:58. LibDoc 4.6.0.0-r.29The content file ABB_DataLogger_AC500.json was generated with Automation Builder 2.7 on 21.11.2023, 17:05:22.