LogGeneric_Input (FB)

FUNCTION_BLOCK LogGeneric_Input EXTENDS AbbLConCA

This function at the same time, can write Datasets of type BOOL, BYTE, INT, UINT, DINT, UDINT and REAL with different length of 27…88 values (depending on type) are stored as Format *.csv in SRAM-FIFOin of Data logger

The Function Block writes datasets in the SRAM-FIFOin of the controller and doesn’t send them directly to a central control station. This is done by the user. With the Function Block LogGeneric_Output the data to be sent are provided as an interface.

../../../../../_images/LogGeneric_Input.jpg
InOut:

Scope

Name

Type

Initial

Comment

Input

Send

BOOL

2: Start a send request on raising edge

Cycle

BOOL

3: Perform a cyclic send each scandown cycle. At Scandown=0 a dataset is written in each cycle

Auto

BOOL

4: With each change of an input value or exceeding/falling down of Threshold, this input writes a dataset in FIFOin

Scandown

UINT

5: On cyclic send only send in each <scandown< cycle
  • e.g. Scandown = 100: every hundredth cycle writes a value in FifoIn

  • e.g. Scandown = 0: in every cycle a dataset is written

ThresholdRefresh

BOOL

6: Threshold refresh. FALSE: refresh each thresholds separately. TRUE: refresh all thresholds together when one threshold reached

Id

STRING(8)

7: Sender Identity - maximum 8 character, freely selectable name/text

DataType

BYTE

8: Possible Data types: 1=BOOL, 2=BYTE, 3=INT, 4=UINT, 5=DINT, 6=UDINT, 7=REAL

Length

INT

9: Current length of Data. Maximum value 88

Threshold

POINTER TO DINT

10: When exceeding or falling below a threshold, a writing operation of a dataset into the FIFOin is started.

After this operation, either only the single threshold difference (between input and threshold) is deleted (ThresholdRefresh=FALSE) or all differences (ThresholdRefresh=TRUE). As the input is a poiner to, it has to be connected to an preceding ADR-Operator, to which any available input type can be provided: BOOL, BYTE, INT, UINT, DINT, UDINT, REAL or an array of these data types. Make sure that Threshold is always of the same type as the respective input E.g. if the Input is an ARRAY[0..n] OF BYTE, Threshold has to be an ARRAY[0..n] OF BYTE too. This input is only relevant for 2=BYTE, 3=INT, 4=UINT, 5=DINT, 6=UDINT, 7=REAL, not for bool. For the BOOL type inputs, Threshold is not needed.

Data

POINTER TO DINT

11: Address of Data (ARRAY or VALUE with ADR on Data of FB)

Input value as single value or as ARRAY for the possible values. As the input is a POINTER TO, it has to be connected to a preceding ADR-Operator, to which any available input-type can be provided: BOOL, BYTE, INT, UINT, DINT, UDINT, REAL or an ARRAY of these data types

Output

ErrorID

ERROR_ID

NO_ERROR

3: Shows error, Refer ERROR_ID enumeration for details of the error

State

zLOG_ENUM_STATE

zLOG_IDLE

4: Actual state of LogInput, enumeration of Type zLOG_ENUM_STATE

InExecution

BOOL

FALSE

5: A command was received when InExecution=TRUE - write datasets is carried out

Overflow

BOOL

FALSE

6: Overflow, FIFOin is full, datasets are rejected. Output will be TRUE, if an overflow occurs. On this output a rising edge (FALSE -> TRUE) shows that communication/logging request occurred too fast and therefore the SRAM-FIFOin is full

FifoInLevel

DINT

0

7: Level FIFOin (0…161)

FifoInNextWrite

DINT

0

8: Next write position in FIFOin

FifoInMaxLimit

DINT

0

9: Maximum limit of FIFOin - Standard value 161

NumberItems

DINT

0

10: Number of Items since Enable=TRUE

NumberOverflow

DINT

0

11: Number of Overflow items since Enable=TRUE

Methods:

A_StartAction

B_CyclicAction

D_AbortAction

E_ResetAction

Structure: