HaModTon (FB)
FUNCTION_BLOCK HaModTon
Function block HaModTon is a standard On delay timer with automatic data synchronization in a high availability system Only internal variables and outputs are synchronized. Input variables and parameters are not synchronized. If needed, use HaModDataSync to achieve the same.
Note
It is not recommended to call utility blocks inside other function blocks in user application, this can impact the data synchronization between PLCs. For example, if HaModTon function block is used inside user’s function block, it will lead to data sync mismatch.
- InOut:
Scope
Name
Type
Initial
Comment
Input
InBOOLFALSE
1:Starts timer with rising edge, resets timer with falling edge
PtTIMETIME#0ms
2:Time to pass, before Q is set
Output
QBOOL1:Is TRUE, Pt seconds after In had a rising edge
EtTIME2:Elapsed time