HaModIntegral (FB)
FUNCTION_BLOCK HaModIntegral
Function block HaModIntegral is a standard integral with automatic data synchronization in a high availability system Only internal variables and outputs are synchronized. Input variables and parameters are not synchronized. If needed, use HaModDataSync to achieve the same.
Note
It is not recommended to call utility blocks inside other function blocks in user application, this can impact the data synchronization between PLCs. For example, if HaModTon function block is used inside user’s function block, it will lead to data sync mismatch.
- InOut:
Scope
Name
Type
Initial
Comment
Input
InREAL0
1:Input variable
TmDINT0
2:Time since last call in msec
ResetBOOLFALSE
3:Reset: Out is set to zero and Overflow to false
Output
OutREAL0
1:Value of the integral
OverflowBOOLFALSE
2:Overflow