HaModCtud (FB)

FUNCTION_BLOCK HaModCtud

Function block HaModCtud is a standard up and down counter with automatic data synchronization in a high availability system QV is TRUE, if counter is 0. QU is TRUE, if counter is PV Only internal variables and outputs are synchronized. Input variables and parameters are not synchronized. If needed, use HaModDataSync to achieve the same.

Note

It is not recommended to call utility blocks inside other function blocks in user application, this can impact the data synchronization between PLCs. For example, if HaModTon function block is used inside user’s function block, it will lead to data sync mismatch.

InOut:

Scope

Name

Type

Initial

Comment

Input

Cu

BOOL

FALSE

1:Count Up

Cd

BOOL

FALSE

2:Count Down

Reset

BOOL

FALSE

3:Reset Counter to Null

Load

BOOL

FALSE

4:Load Start Value

Pv

WORD

0

5:Start Value / Counter Limit

Output

Qu

BOOL

FALSE

1:Counter reached Limit

Qd

BOOL

FALSE

2:Counter reached Null

Cv

WORD

0

3:Current Counter Value