Using a basic sample project below, you will find the most important steps and options for configuring and running a static analysis.
Requirements: CODESYS Static Analysis is installed.
Sample project
If you want to reproduce the example project, create a standard project and insert the POUs below the application in the device tree. Then configure the communication settings for the connection to your local CODESYS Control Win V3.
FUNCTION_BLOCK fb1
VAR_INPUT
iVar_fb1in1 : INT;
ivar_fb1in2 : INT;
rVar_fb1in3 : REAL;
END_VAR
VAR_OUTPUT
iVar_fb1out:INT;
END_VAR
VAR
P_fSampleProperty : INT;
rVar : REAL;
PRO : BOOL;
END_VAR
iVar_fb1out:=iVar_fb1in1 + 1;
FUNCTION_BLOCK fb2
VAR_INPUT
iVar_fb2in:INT;
END_VAR
VAR_OUTPUT
iVar_fb2out:INT;
END_VAR
VAR
END_VAR
PROGRAM PLC_PRG
VAR
fb1_inst: fb1;
fb2_inst: fb2;
END_VAR
fb1_inst(iVar_fb1in1 := 99);
fb2_inst(iVar_fb2in := 22);
fb2_inst(iVar_fb2in := 1);
Checking for compliance to rules
-
Click “Build Static Analysis Settings”. Switch to the “Rules” tab.
A list is displayed containing all possible rule checks. They are organized in a tree structure by topical category. The rule number is added in parentheses (for example, “Unused variables (33)” in category “Unused objects”).
-
Click the check box of the first line a few times (“Rules” node).
Clicking toggles the activation status. The check boxes in the entire tree have a red or orange check mark, or no check mark at all.
-
In this way, activate all entries with a red check mark. This means that CODESYS Static Analysis should report any detected rule violations as errors.
-
Click “Build Static Analysis Run Static Analysis”.
Errors are reported in the message view. The message texts are tagged with a
and begin with the error number "SA<rule number>". -
Double-click the first message
SA0033: Unused variables 'iVar_fb2out'.The focus moves to the declaration part of function block
fb2and the relevant variable is selected. The variable is declared, but not used. This is checked in Rule 33 (“Unused variables”). In the code, the relevant locations are underlined with a wavy line. -
To test the automatic execution of the analysis, click “Build Static Analysis Settings”. On the “Settings” tab, select the “Perform static analysis automatically” option. Click “OK” to exit the dialog.
-
Click “Online Login”.
A dialog prompt indicates that compile errors exist. The errors reported by the code analysis are displayed again in the message view.
-
Click “Build Static Analysis Settings”. Switch to the “Rules” tab.Now clear all of the rules in the dialog. In the “Unused Objects” category, explicitly activate Rule SA0035 (“Unused input variables (35)”) with an orange-colored check mark to report a warning. See the tooltip for the rule text: “This rule corresponds to the following PLCopen rules: CP24”). Click “OK” to exit the dialog.
In the project settings, click “OK”.
-
Click “Build Generate Code”.
The analysis is performed automatically. Two errors are reported in the message view:
§ SA0035: Unused input variable 'iVar_fb1in2and§ SA0035: Unused input variable 'iVar_fb1in3. -
Double-click the message and comment or remove the declaration. Perform the code analysis again.
No error messages are displayed.
Checking for compliance to defined naming conventions
-
Click “Build Static Analysis Settings”. Click the “Naming Conventions” tab.
You see a table in a tree structure that is divided into expandable categories of variables and program blocks.
-
Expand the “Prefixes for Variables” - “Prefixes for Types” category, and in the “Prefix” column, specify
Ifor “INT (14)”.Expand the “Prefixes for POUs” - “Prefixes for POU Type” category: In the “Prefix”column, specify the
progfor “PROGRAM (122)” andfbfor “FUNCTIONBLOCK (103)”. -
Select the “First character after prefix should be an upper case letter” option. Clear all other options.
-
Click “Build Static Analysis Run Static Analysis”.
Error messages:
-
NC0102: Invalid name 'PLC_PRG': Expect prefix 'prog'because PLC_PRG does not have the required prefix -
First character after prefix should be uppercase: 'ivar_fb1in2'becauseivar_fb1in2 : INT;infb1 -
NC0014: Invalid variable name P_fSampleProperty: Expect prefix 'i'because this integer variable does not have the required prefix
-
Checking for forbidden symbols
-
Click “Build Static Analysis Settings”. Click the “Forbidden Symbols” tab.
A line editor allows for specifying character strings that should not to be used in the code.
-
As an example, double-click the blank line and type in the invalid character string
PROdirectly. Double-click the next blank line and click
to open the input assistance. From “Standard Types”, select “REAL”. Click “OK” to exit the dialog. -
Click “Build Static Analysis Run Static Analysis”.
The error messages
Forbidden symbol 'REAL'andForbidden symbol 'PRO'are displayed in the message view. Double-click the message text to jump to the relevant line of code.
Displaying of metrics
CODESYS Static Analysis performs selected tests on the code, and you can display the results in a view.
-
Click “Build Static Analysis Settings”. Click the “Metrics” tab.
The metrics that CODESYS Static Analysis applies to the code are listed in a table.
-
For this example, activate the “Number of inputs variables” metric and specify the permitted range of values: lower limit
1and upper limit2. Activate some more metrics, for example “Code size” and “Number of calls”. -
Click “Build Static Analysis View Standard Metrics”.
The view includes a table with a line for each “Program unit” of the sample program. For each activated metric, there is a column showing the measured values. Values that are outside of the range of values defined in the settings are highlighted in red. In the case of this specific example, this is at least the “PLC_PRG/Inputs” field because the number of input variables in this POU is greater than the defined upper limit of
2.
See also