Function: In the dialog, you select automatic static analysis, and save or load the project settings for static analysis as a CSA file.
Call:
-
Menu bar: “Project Project Settings”, “Static Analysis” category, “Open configuration dialog” link
-
Menu bar: “Build Static analysis Settings”
Requirement:
-
The CODESYS Static Analysis package is installed.
-
A project is open.
|
“Perform static analysis automatically” |
|
|
“Load” |
Opens the “Load Static Analysis Configuration” dialog for selecting the project settings for the static analysis as a CSA file in the file system. When you click the “Open” button, the selected CSA file is loaded. |
|
“Save” |
Opens the “Save Static Analysis Configuration” dialog for saving all project settings in the “Static Analysis” category as a CSA file in the file system. |
:
: The code check is not performed automatically, but it can be performed explicitly
by means of the