Function: In the dialog, you select the rules that are checked during the static analysis of the source code of a project.
Call:
-
Menu bar: “Project Project Settings”, “Static Analysis” category, “Open configuration dialog” link
-
Menu bar: “Build Static analysis Settings”
Requirement:
-
The CODESYS Static Analysis package is installed.
-
A project is open.
This tab shows a tree structure of all rules that can be checked during static analysis. By default, every rule is activated, with the exception of SA0016, SA0024, SA0073, SA0101, SA0105, SA0106, SA0133, SA0134, SA0150, SA0162, and all strict IEC rules.
Each rule has a unique number. When the rule is checked and a violation is detected, the rule number and an error description are shown in the message view in the “Build” category in the following format: SA<rule number>, where SA stands for "Static Analysis" (example: "SA003" for rule 3).
The list of available rules can be extended by specific plug-ins.
|
Some rules that are activated in the dialog can be deactivated temporarily in the application by applying a pragma. |
|
|
When you click the check box, the setting toggles between When you activate or deactivate a parent node, all child rules are also activated or deactivated, respectively. |
|
|
“Filter”: |
|
|
Columns |
|
|
“Rules” |
List of rules with rule number |
|
Rule check |
|
|
“Precompile” |
Rules which can be checked during precompile are identified by a check mark An immediate bugfix (Quickfix) is possible for these rules. You can execute an automatic, immediate error handling directly at the affected code positions. |
|
“Rule specific configuration” |
For some rules, you can double-click the field to open a rule-specific dialog to configure the rule. |
|
“Importance”: |
Importance of the rule:
|
,
, and
.
: Rules are grouped by category.
: Rules are displayed as a flat list. By clicking on the corresponding column header,
the list can be sorted by rule number, activation/deactivation, rule-specific configuration,
or importance.
) for the static analysis is displayed in the message view.
) for the static analysis is displayed in the message view.
in this column.