MC_SetOverride (FB)
FUNCTION_BLOCK MC_SetOverride
This function block sets the values of override for the whole axis and all functions that are working on that axis.
The override parameters act as a factor that is multiplied to the commanded velocity, acceleration, deceleration and jerk of the move function block.
The input AccFactor acts on positive and negative acceleration (deceleration).
This function block sets the factor. The override factor is valid until a new override is set.
The default values of the override factors are 1.0.
The value of the overrides can be between 0.0 and 1.0. Values > 1.0 and values < 0.0 are not allowed. The value 0.0 is not allowed for AccFactor and JerkFactor.
Override does not act on slave axes. (Axes in the state Synchronized Motion).
The function block does not influence the single axis state diagram.
The override factors are just effective to modify the velocity, acceleration, deceleration and jerk which are provided as explicit values by PLCopen function blocks. They do not modify a movement which is commanded by other means as camming, gearing, profiling, where no explicit velocity, acceleration, deceleration and jerk is in place
- InOut:
Scope
Name
Type
Initial
Comment
Input
EnableBOOLIf TRUE, it writes the value of the override factor continuously. If FALSE it should keep the last value
VelFactorLREAL1
New override factor for the velocity, Range: =0.0, >0.0, <5.0
AccFactorLREAL1
New override factor for the acceleration or deceleration, Range: >0.0, < 5.0
JerkFactorLREAL1
New override factor for the jerk, Range: >0.0, <5.0
Output
EnabledBOOLThe block is enabled and working
ErrorBOOLSignals that error has occurred within function block
ErrorIDError identification. For error details refer to Enumeration ERROR_ID
Inout
AxisReference to axis