MC_ReadBoolParameter (FB)
FUNCTION_BLOCK MC_ReadBoolParameter
It will support the Parameters defined as “standard” in the PLCopen. These parameters will be transferred to the units as used for PLCopen function blocks
When a drive based axis implementation is used, the function block returns the value of a drive specific BOOL parameter or a PLCopen BOOL parameter. When the Central Motion Control axis implementation is used, a BOOL parameter according to the list PLCopen parameter is returned
Parameter No(PN) |
Name |
DataType |
Min. |
Max. |
Default |
R/W |
Comments |
|---|---|---|---|---|---|---|---|
1 |
CommandedPosition |
DINT |
R |
Commanded Position |
|||
2 |
SWLimitPos |
DINT |
-2147483647 |
2147483647 |
2147483647 |
R/W |
Positive Software limit switch position |
3 |
SWLimitNeg |
DINT |
-2147483647 |
2147483647 |
-2147483647 |
R/W |
Negative Software limit switch position |
4 |
EnableLimitPos |
BOOL |
FALSE |
TRUE |
FALSE |
R/W |
Enable positive software limit switch |
5 |
EnableLimitNeg |
BOOL |
FALSE |
TRUE |
FALSE |
R/W |
Enable negative software limit switch |
6 |
EnablePostLagMonitoring |
BOOL |
FALSE |
TRUE |
TRUE |
R/W |
Enable monitoring of position lag (following error) |
7 |
MaxPositionLag |
DINT |
1 |
2147483647*** |
R |
Maximal position lag |
|
8 |
MaxVelocitySystem |
DINT |
32767 |
R |
Maximal allowed velocity of the axis in the motion system |
||
9 |
MaxVelocityAppl |
DINT |
0** |
32767 |
32767 |
R/W |
Maximal allowed velocity of the axis in the application |
10 |
ActualVelocity |
DINT |
-32767 |
32767 |
R |
Actual velocity |
|
11 |
CommandedVelocity |
DINT |
-32767 |
32767 |
R |
Commanded Velocity |
|
12 |
MaxAccelerationSystem |
DINT |
32767 |
R |
Maximal allowed acceleration of the axis in the motion system |
||
13 |
MaxAccelerationAppl |
DINT |
10 |
32767 |
32767 |
R/W |
Maximal allowed acceleration of the axis in the application |
14 |
MaxDecelerationSystem |
DINT |
32767 |
R |
Maximal allowed deceleration of the axis |
||
15 |
MaxDecelerationAppl |
DINT |
10 |
32767 |
32767 |
R/W |
Maximal allowed deceleration of the axis |
16 |
MaxJerk |
DINT |
0* |
2147483647 |
2147483647 |
R/W |
Maximal allowed jerk of the axis |
2001 |
MODULO_NOMINATOR |
DINT |
1 |
2147483647 |
1 |
R/W |
ABB specific parameter. Used for Central Motion Control implementation: Gearbox modifier to MODULO_RANGE |
2002 |
MODULO_DENOMINATOR |
DINT |
1 |
2147483647 |
1 |
R/W |
ABB specific parameter. Used for Central Motion Control implementation: Gearbox modifier to MODULO_RANGE |
2003 |
EnableLimit2Decelerate |
BOOL |
FALSE |
TRUE |
FALSE |
R/W |
Enable software limit switches to decelerate |
2004 |
EnableLimitAbort |
BOOL |
FALSE |
TRUE |
FALSE |
R/W |
Enable that software limit switches will abort ongoing movement |
2005 |
EnableLimitVelocity |
BOOL |
FALSE |
TRUE |
FALSE |
R/W |
If the velocity is limited the unmoved position will be covered whenever possible |
2006 |
SWLimit2DecPos |
LREAL |
-2147483647 |
2147483647 |
2147483647 |
R/W |
Used as end position for EnableLimit2Decelerate |
2007 |
SWLimit2DecNeg |
LREAL |
-2147483647 |
2147483647 |
2147483647 |
R/W |
Used as end position for EnableLimit2Decelerate |
2008 |
MaxPositionGapLL |
LREAL |
0 |
214748364700 |
0 |
R/W |
Used to stop the ongoing movement if position is behind |
*0 means: no limitation of jerk is performed.
**Axis will stay in stop.
***Is modified by CMC_Axis_Control_Parameter, the maximum Value is calculated in increments, the value which is delivered by ReadParameter will be given in [u].
- InOut:
Scope
Name
Type
Comment
Input
EnableBOOLRead continuously on “TRUE”
ParameterNumberWORDNumber of the parameter
Output
ValidBOOLValue is available
BusyBOOLThe function block with Busy = TRUE has control on the axis
ErrorBOOLSignals that error has occurred within function block
ErrorIDError identification. For error details refer to Enumeration ERROR_ID
ValueBOOLValue of the specified parameter in the datatype
Inout
AxisReference to axis