MC_ReadParameter (FB)

FUNCTION_BLOCK MC_ReadParameter

It will support the Parameters defined as “standard” in the PLCopen. These parameters will be transferred to the units as used for PLCopen function blocks

../../../../../../_images/plcopen.png

When a drive based axis implementation is used, the function block returns the value of a drive specific parameter or a PLCopen parameter. When the Central Motion Control axis implementation is used, a parameter according to the list PLCopen parameter is returned

Parameter No(PN)

Name

DataType

Min.

Max.

Default

R/W

Comments

1

CommandedPosition

DINT

R

Commanded Position

2

SWLimitPos

DINT

-2147483647

2147483647

2147483647

R/W

Positive Software limit switch position

3

SWLimitNeg

DINT

-2147483647

2147483647

-2147483647

R/W

Negative Software limit switch position

4

EnableLimitPos

BOOL

FALSE

TRUE

FALSE

R/W

Enable positive software limit switch

5

EnableLimitNeg

BOOL

FALSE

TRUE

FALSE

R/W

Enable negative software limit switch

6

EnablePostLagMonitoring

BOOL

FALSE

TRUE

TRUE

R/W

Enable monitoring of position lag (following error)

7

MaxPositionLag

DINT

1

2147483647***

R

Maximal position lag

8

MaxVelocitySystem

DINT

32767

R

Maximal allowed velocity of the axis in the motion system

9

MaxVelocityAppl

DINT

0**

32767

32767

R/W

Maximal allowed velocity of the axis in the application

10

ActualVelocity

DINT

-32767

32767

R

Actual velocity

11

CommandedVelocity

DINT

-32767

32767

R

Commanded Velocity

12

MaxAccelerationSystem

DINT

32767

R

Maximal allowed acceleration of the axis in the motion system

13

MaxAccelerationAppl

DINT

10

32767

32767

R/W

Maximal allowed acceleration of the axis in the application

14

MaxDecelerationSystem

DINT

32767

R

Maximal allowed deceleration of the axis

15

MaxDecelerationAppl

DINT

10

32767

32767

R/W

Maximal allowed deceleration of the axis

16

MaxJerk

DINT

0*

2147483647

2147483647

R/W

Maximal allowed jerk of the axis

2001

MODULO_NOMINATOR

DINT

1

2147483647

1

R/W

ABB specific parameter. Used for Central Motion Control implementation: Gearbox modifier to MODULO_RANGE

2002

MODULO_DENOMINATOR

DINT

1

2147483647

1

R/W

ABB specific parameter. Used for Central Motion Control implementation: Gearbox modifier to MODULO_RANGE

2003

EnableLimit2Decelerate

BOOL

FALSE

TRUE

FALSE

R/W

Enable software limit switches to decelerate

2004

EnableLimitAbort

BOOL

FALSE

TRUE

FALSE

R/W

Enable that software limit switches will abort ongoing movement

2005

EnableLimitVelocity

BOOL

FALSE

TRUE

FALSE

R/W

If the velocity is limited the unmoved position will be covered whenever possible

2006

SWLimit2DecPos

LREAL

-2147483647

2147483647

2147483647

R/W

Used as end position for EnableLimit2Decelerate

2007

SWLimit2DecNeg

LREAL

-2147483647

2147483647

2147483647

R/W

Used as end position for EnableLimit2Decelerate

2008

MaxPositionGapLL

LREAL

0

214748364700

0

R/W

Used to stop the ongoing movement if position is behind

*0 means: no limitation of jerk is performed.

**Axis will stay in stop.

***Is modified by CMC_Axis_Control_Parameter, the maximum Value is calculated in increments, the value which is delivered by ReadParameter will be given in [u].

InOut:

Scope

Name

Type

Comment

Input

Enable

BOOL

Read continuously on “TRUE”

ParameterNumber

WORD

Number of the parameter

Output

Valid

BOOL

Value is available

Busy

BOOL

The function block with Busy = TRUE has control on the axis

Error

BOOL

Signals that error has occurred within function block

ErrorID

ERROR_ID

Error identification. For error details refer to Enumeration ERROR_ID

Value

DINT

Value of the specified parameter in the datatype

Inout

Axis

Axis_Ref

Reference to axis