Redundancy Implementation (LIB)

Version

3.5.21.0

Author

CODESYS Development GmbH

Placeholder

Redundancy Implementation

Description 1

This library contalins external interface functions for the redundancy component of the runtime system. The redundancy component allows connecting two CODESYS PLCs to create one redundant system.

Contents:

Indices and tables

1
Based on Redundancy Implementation.library, last modified 10.03.2025, 15:58:55. LibDoc 4.6.0.0-r.29
The content file Redundancy Implementation.library.json was generated with CODESYS V3.5 SP16 Patch 3 on 10.03.2025, 15:58:57.