Redundancy (LIB)

Version

3.5.17.0

Namespace

RDCY

Author

3S - Smart Software Solutions GmbH

Placeholder

Redundancy

Description 1

This library provides access to the redundancy component of the runtime system. The redundancy component allows connecting two CODESYS PLCs to create one redundant system.

Indices and tables

1
Based on Redundancy.library, last modified 20.04.2021, 16:00:53. LibDoc 4.6.0.0-r.29
The content file Redundancy.library.json was generated with CODESYS V3.5 SP16 Patch 3 on 20.04.2021, 16:00:53.