RdcyAcyclicRegisterUsage (FUN)
FUNCTION RdcyAcyclicRegisterUsage : RTS_IEC_RESULT
Register a usage for the acyclic redundancy interface. Use the event handle returned in the hEvent parameter for registering your callback function for the EVT_RdcyAcyclicRecv event. Precondition: The acyclic data transfer module has to have reached at least the RA_STATE_INITIALIZED RdcyAcyclicState. Hint: The current state of the acyclic data transfer module can be queried with the RdcyAcyclicGetCurState FUNCTION.
- InOut:
Scope
Name
Type
Comment
Return
RdcyAcyclicRegisterUsageRTS_IEC_RESULTError code (see CmpErrors.library). ERR_DUPLICATE if data name is not unique, ERR_NOTINITIALIZED if the acyclic data transfer module has not yet reached the RA_STATE_INITIALIZED RdcyAcyclicState, ERR_PARAMETER if one of the parameters is invalid, ERR_FAILED if the event could not be created or the MemBlockDictBock could not be created, else ERR_OK
Input
pcszAcyclicDataUUIDREFERENCE TO STRING
Data UUID (AKA data GUID) in textual representation. The size is 37 bytes (36 characters, plus ‘0’). As per RFC 9562, the UUID is represented as hexadecimal values in the 8-4-4-4-12 format, xxxxxxxx-xxxx-xxxx-xxxx-xxxxxxxxxxxx, where every x represents 4 bits. Note that the alphabetic characters may be all uppercase, all lowercase, or mixed case. An example string using this UUID format: f81d4fae-7dec-11d0-a765-00a0c91e6bf6
pEventIDPOINTER TO DWORD
Output: Pointer to the EVENTID of the event with the hEvent handle.
phEventPOINTER TO RTS_IEC_HANDLE
Output: Pointer to the event handle. To be used for the EventRegisterCallbackFunction function of the CmpEventMgr library.