RdcyAcyclicUnregisterUsage (FUN)
FUNCTION RdcyAcyclicUnregisterUsage : RTS_IEC_RESULT
Unregister a usage from the acyclic redundancy interface. Precondition: The acyclic data transfer module has to have reached at least the RA_STATE_INITIALIZED RdcyAcyclicState. Hint: The current state of the acyclic data transfer module can be queried with the RdcyAcyclicGetCurState FUNCTION.
- InOut:
Scope
Name
Type
Comment
Return
RdcyAcyclicUnregisterUsageRTS_IEC_RESULTError code (see CmpErrors.library). ERR_NO_OBJECT if the usage handle is unknown, ERR_NOTINITIALIZED if the acyclic data transfer module has not yet reached the RA_STATE_INITIALIZED RdcyAcyclicState, ERR_PARAMETER if pcszAcyclicDataUUID is NULL or doesn’t contain a valid UUID format, else ERR_OK
Input
pcszAcyclicDataUUIDREFERENCE TO STRING
The same Data UUID, which was used for registration with the RdcyAcyclicRegisterUsage FUNCTION.