TrendFbTrendStorageWriterReader.Initialize (METH)
METHOD Initialize
This method has to be called once before using the current instance
- InOut:
Scope
Name
Type
Comment
Input
udiCountSamplesUDINTThe maximum number of samples, that have to be read and passed to the attached ITraceMgrPacketReaderClient instance.
itfTraceMgrPacketReaderClientITraceMgrPacketReaderClientThe ITraceMgrPacketReaderClient instance, that processes the data read from the trend storage.
traceMgrPacketVisuStructTraceMgrPacketA VisuStructTraceMgrPacket variable, where the description of the ITraceMgrPacket and its variables read from the trend storage will be stored and passed to ITraceMgrPacketReaderClient instance.
itfTrendRootPageManagerAn already initialized instance of ITrendRootPageManager, that is able to provide the root pages for tables and indexes