ITrendRootPageManager2.DetermineRootPagesTimeout (METH)

METHOD DetermineRootPagesTimeout : STO.ERROR

This method has to be called once to determine the rootpages of the database

InOut:

Scope

Name

Type

Comment

Return

DetermineRootPagesTimeout

STO.ERROR

Input

itfTraceMgrPacket

ITraceMgrPacket

An instance of ITraceMgrPacket describing the packet that is currently running in the runtime system

tMaxWaitTime

TIME

Roughly the maximal interval that this method must block while waiting for determination of the root pages.