ITimestampTraverserClient.ProcessVariableForTimestamp (METH)

METHOD ProcessVariableForTimestamp

Notfication for ITimestampTraverserClient instance, that a variable for the current timestamp has to be processed.

InOut:

Scope

Name

Type

Comment

Input

itfTraceMgrVariable

ITraceMgrVariable

The ITraceMgrVariable for which the variable value belongs to

iRecordIndex

INT

The 0 relative index of the ITraceMgrVariable within all variables

pbyByte

POINTER TO BYTE

Points to the corresponding location in memory, where the data (i.e. the variable value) is located.