F_Parameter (STRUCT)
TYPE F_Parameter : STRUCT
F-Parameters of a PROFIsafe device.
- InOut:
Name
Type
Comment
F_Check_SeqNrBOOLV2-mode: ignore, Reserved by legacy mode
F_Check_iParBOOLManufacturer specific use within homogeneous systems
F_SILConfigured SIL
F_CRC_LengthCRC2 signature length
F_CRC_SeedBOOLUse of different rules for CRC seed value and MNR for the CRC2 signature calculation
F_PassivationBOOLF-(Sub)Module or Channel-granular Passivation
F_Block_IDParameter block type identification
F_Par_VersionVersion No. of F-Parameters/FSCP 3/1 operational mode
F_Source_AddressUINTF source address
F_Dest_AddressUINTF destination address
F_WD_TimeUINTWatchdog time in the F driver
F_WD_Time_2UINTOptional secondary watchdog time in F-(Sub)Modules designed for Dynamic Reconfiguration or maintenance of fault tolerant systems or Parameterization in Run.
F_iPar_CRCUDINTValue of the iParameter CRC signature calculation
F_Par_CRCUINTCRC signature calculation across the F-Parameters