ETC_CO_SdoInfoGeEntryDescription (FB)

FUNCTION_BLOCK ETC_CO_SdoInfoGeEntryDescription

InOut:

Scope

Name

Type

Initial

Comment

Input

xExecute

BOOL

Rising edge: ACTION starts Falling edge: Resets outputs If a falling edge occurs before the function block has completed its action, the outputs operate in the usual manner and are only reset if either the action is completed or in the event of an error. In this case, the corresponding output values (xDone, xError) are present at the outputs for exactly one cycle.

xAbort

BOOL

FALSE

TRUE: Action is stopped immediately and all outputs are reset to their initial values.

usiCom

USINT

1

Index of master 1: first ETC master

uiDevice

UINT

the physical slave address to access the EtherCAT slave

wIndex

WORD

The index of the CoE object

bySubIndex

BYTE

The sub index of the CoE object

byValueInfo

BYTE

The value info include which elements shall be in te response Bit 0: reserved Bit 1: reserved Bit 2: reserved Bit 3: unit type Bit 4: default value Bit 5: minimum value Bit 7: maximum value

udiTimeOut

UDINT

Timeout for operation in ms

Output

xDone

BOOL

TRUE: Action successfully completed

xBusy

BOOL

TRUE: Function block active

xError

BOOL

TRUE: Error occurred, function block aborts action, FALSE: No error

eError

ETC_CO_ERROR

If xError is true then eError shows the error reason

wDataType

WORD

Datatype of entry

wBitLength

WORD

Size of entry in bits

wObjectAccess

WORD

acess flast of object

pData

POINTER TO BYTE

Pointer to received data

szDataLength

CAA.SIZE

Size of received data