ETC_CO_SdoWriteDWord (FB)

FUNCTION_BLOCK ETC_CO_SdoWriteDWord

Like ETC_CO_SdoWrite4, this function block is for writing EtherCAT slave parameters. However, the data to be written are transferred not as an array, but in a DWORD (dwData). If byte swapping is necessary it is carried out automatically. The value to be written can thus be specified directly.

InOut:

Scope

Name

Type

Initial

Comment

Input

xExecute

BOOL

Rising edge: ACTION starts Falling edge: Resets outputs If a falling edge occurs before the function block has completed its action, the outputs operate in the usual manner and are only reset if either the action is completed or in the event of an error. In this case, the corresponding output values (xDone, xError) are present at the outputs for exactly one cycle.

xAbort

BOOL

FALSE

TRUE: Action is stopped immediately and all outputs are reset to their initial values.

usiCom

USINT

1

Index of master 1: first ETC master

uiDevice

UINT

The physical slave address to access the EtherCAT slave

usiChannel

USINT

1

not used in the moment because channel is set automatically

wIndex

WORD

The index of the CoE object

bySubindex

BYTE

The sub index of the CoE object

udiTimeOut

UDINT

Timeout for operation in ms

dwData

DWORD

The data to be written

usiDataLength

USINT

Number of bytes to be written

Output

xDone

BOOL

TRUE: Action successfully completed

xBusy

BOOL

TRUE: Function block active

xError

BOOL

TRUE: Error occurred, function block aborts action, FALSE: No error

eError

ETC_CO_ERROR

If xError is true then eError shows the error reason

udiSdoAbort

UDINT

The abort code as received from the slave device