StaticCredentialsProvider.StartGetCredentials (METH)

METHOD StartGetCredentials : __UXINT

Will return an id of the question for credentials. This id can be used in the following calls to |ICredentialsProvider.IsGetCredentialsFinished|

InOut:

Scope

Name

Type

Comment

Return

StartGetCredentials

__UXINT

Input

pstDataSource

POINTER TO STRING

The name of the datasource to request credentials for. Can be used as an informative hint to the user for example.

Output

udiErrorCode

SysTypes.RTS_IEC_RESULT

An error code representing the result of this operation. In case of ERR_PENDING there will be further calls to this method.