StaticCredentialsProvider.IsGetCredentialsFinished (METH)

METHOD IsGetCredentialsFinished : SysTypes.RTS_IEC_RESULT

Will return ERR_OK if the request is finished, ERR_PENDING if it is not yet finished, ERR_DS_RETRYLOGIN if the login should be tried again, another error code in case of an error

InOut:

Scope

Name

Type

Comment

Return

IsGetCredentialsFinished

SysTypes.RTS_IEC_RESULT

Input

uxiRequestId

__UXINT

The request id to check the result for