StaticCredentialsProvider.GetCredentials (METH)
METHOD GetCredentials : SysTypes.RTS_IEC_RESULT
Must return ERR_OK if called after a successfull |ICredentialsProvider.IsGetCredentialsFinished|
- InOut:
Scope
Name
Type
Comment
Return
GetCredentialsSysTypes.RTS_IEC_RESULTInput
uxiRequestId__UXINTThe request id to get the credentials for
Output
credentialsIDatasources.ICredentialsThe resulting credentials of the current implementation.
Note
Please remark that the returned object is not required to be alive longer than to the next calls on this object using the interface |ICredentialsProvider|