Write (FB; Prefix filwr)
FUNCTION_BLOCK Write EXTENDS CBM.ETrigToA
pBuffer” should not be modified during the write action! The size of the structure of the memory containing the bytes to be written
as well as the number of bytes to be written will not be checked.- InOut:
Scope
Name
Type
Comment
Inherited from
Input
xExecuteBOOLRising edge: Action startsFalling edge: Resets outputsIf a falling edge occurs before the function block has completed its action, the outputs operate in the usual manner and are only reset if either the action is completed or in the event of an error. In this case, the corresponding output values (xDone,xError) are present at the outputs for exactly one cycle.ETrigToA
xAbortBOOLTRUE: Action is stopped immediately and all outputs are reset to their initial values.ETrigToA
udiTimeOutUDINTDefines the time (µs) after which an FB (e.g. requiring an external acknowledgement) aborts operation due to a timeout with error message.
ETrigToA
Output
xDoneBOOLTRUE: Action successfully completedETrigToA
xBusyBOOLTRUE: Function block activeETrigToA
xErrorBOOLTRUE: Error occurred, function block aborts actionFALSE: No errorETrigToA
xAbortedBOOLTRUE: Action aborted by userETrigToA
Input
hFileCAA.HANDLEFile handle
pBufferCAA.PVOIDThe address from where the data can be obtained, can be determined with the help of operator ADR.
szSizeCAA.SIZENumber of bytes to be written (can be determined via operator SIZEOF)
Output
eErrorLocal library error ID (0: no error; 5101: time out)