Copy (FB; Prefix filcp)
FUNCTION_BLOCK Copy EXTENDS CBM.ETrigToA
xOverWrite”. If the overwrite mode is activated, no write protection may be activated in the existing file.- InOut:
Scope
Name
Type
Initial
Comment
Inherited from
Input
xExecuteBOOLRising edge: Action startsFalling edge: Resets outputsIf a falling edge occurs before the function block has completed its action, the outputs operate in the usual manner and are only reset if either the action is completed or in the event of an error. In this case, the corresponding output values (xDone,xError) are present at the outputs for exactly one cycle.ETrigToA
xAbortBOOLTRUE: Action is stopped immediately and all outputs are reset to their initial values.ETrigToA
udiTimeOutUDINTDefines the time (µs) after which an FB (e.g. requiring an external acknowledgement) aborts operation due to a timeout with error message.
ETrigToA
Output
xDoneBOOLTRUE: Action successfully completedETrigToA
xBusyBOOLTRUE: Function block activeETrigToA
xErrorBOOLTRUE: Error occurred, function block aborts actionFALSE: No errorETrigToA
xAbortedBOOLTRUE: Action aborted by userETrigToA
Input
sFileNameDestCAA.FILENAMEFile to which data should be copied; for restrictions concerning the file- and directory names see FILE_Open (FB)
sFileNameSourceCAA.FILENAMEFile from which data should be copied, for restrictions concerning the file- and directory names see FILE_Open (FB)
xOverWriteBOOLTRUE
Overwrite an already existing file; TRUE: yes; FALSE: File will not be overwritten, an error message will be created
Output
eErrorLocal library error ID (5105 - FILE_EXIST: Target file already exists; only in case of
xOverWrite := FALSE)szSizeCAA.SIZEsource file size, copied bytes into the destination file